7/11/2018 4:22 AM | |
Joined: 12/18/2014 Last visit: 6/7/2024 Posts: 33164 Rating: (4097)
|
@NIBOU, everything is right and are also interesting information. He does not want to save a LOGO! Program on the SD card, but a LWE project. Edit: That his LOGO! detects that an SD card is plugged, can be recognized by the error message. Diagnostics |
Last edited by: ixo65 at: 7/11/2018 4:35:32 AM |
|
7/11/2018 8:01 AM | |
Posts: 2930 Rating: (432)
|
@erwan84, check Wikipedia (search: FAT32) and read the article. Here you get an explanaition what the problem is. For Linux and Mac there are different driver for formating cards. As you made (together with your friend) use windows PC to format the card (Win7: Fat32 Standard). However , if it still don't work, check: + if you plug in and remove the card switch LOGO! to STOP-Mode + Check if the MSD-card holder if it is pressed in is plan with the LOGO! housing. Some user press in the holder stronlgy and this may result in damadged pins on the holder inside. If this happen, then the holder is not plan with the LOGO! housing. + Insert the MSD.card right: If you look to the front of LOGO!, then the pins of the card must be on the top. Hope this helps |
7/20/2018 6:21 PM | |
Joined: 7/1/2018 Last visit: 10/10/2021 Posts: 11 Rating: (0) |
I think i've tried all now Some person tell me the C indice can be important i took a C10 to try my 8Go was C4.. formated with windows default settings slowly.. Not working neither I even unmount the logo sdcard reader, there's no pins bad.. I found some shop where they say me they were ok to try with a brand new LOGO I'll tell you |
This contribution was helpful to1 thankful Users |
9/26/2019 12:57 AM | |
Joined: 12/10/2010 Last visit: 3/27/2024 Posts: 3 Rating: (0) |
Same issue on me. New LOGO 8 with FAT32 SD card doesn't work. Any solution or suggestion will help. Thanks
|
9/26/2019 3:35 AM | |
Joined: 12/18/2014 Last visit: 6/7/2024 Posts: 33164 Rating: (4097)
|
Everything there is to say is already written in this topic. There is nothing new. - Formatting the microSD card on a Windows PC with FAT32. - Disable the "Quick Formatting" option when formatting. - The maximum size may not exceed 32 GB. - No microSDXC with 64 GB or more. - Check whether the microSD card in the card slot of the LOGO! is inserted correctly. The pins must point upwards. |
This contribution was helpful to1 thankful Users |
9/26/2019 11:14 AM | |
Joined: 9/11/2014 Last visit: 5/29/2024 Posts: 727 Rating: (28) |
Hi, If you are not succesfull, best is: 1. Go to a friend and format the MSD-card on his Windows PC (FAT32) 2. If you do not have a Windows PC, then read the Wikipedia article about FAT32. Here you get an impression what can be different. In this article is also listed what driver for Mac and Linux has to be used to exactly get the needed FAT32. What kind of cards work basically depends on the cluster size. A MSD-card up to 32GB formated in Windows 7 in FAT32 has the right cluster size. All is for good working units and for LOGO! 8. According my experiances a fast formating or "slow" formating is no differents, but may be one. I always use fast formating and never had problems if the card, and the card holder in LOGO! 8 is fine. Hope this helps |
9/26/2019 11:18 AM | |
Joined: 12/18/2014 Last visit: 6/7/2024 Posts: 33164 Rating: (4097)
|
And I used fast format and had problems by some ards. |
9/29/2019 9:27 PM | |
Joined: 3/19/2018 Last visit: 4/28/2024 Posts: 42 Rating: (0) |
I used to have the same problem, a complete (slow) format in FAT32 (in windows 10) solved my problem. |
10/1/2019 8:40 PM | |
Joined: 7/1/2018 Last visit: 10/10/2021 Posts: 11 Rating: (0) |
The little chip who hold the sdcard was not working properly. I had a waranty return and all my sdcards worked directly. Thanks to all |
This contribution was helpful to1 thankful Users |
4/24/2020 1:18 PM | |
Joined: 2/20/2020 Last visit: 6/4/2024 Posts: 2 Rating: (0) |
Thanks a lot sir for valuable support and decription |
4/27/2020 9:55 AM | |
Joined: 8/2/2018 Last visit: 12/16/2023 Posts: 302 Rating: (5) |
Some time the TF card not readable by LOGO. I try remove and reinsert again then it working good now. I think the socket inside LOGO card holder may have some oxidation or dust. If you can not read it every TFcards then you could try spray cleaning agent like CRC degreaser to the inside of socket. If not work then you should request warantee claim to LOGO seller. |
4/27/2020 10:03 AM | |
Joined: 12/18/2014 Last visit: 6/7/2024 Posts: 33164 Rating: (4097)
|
TF card??? You mean mSD card. |
Follow us on