Industry Online Support
Technical Forum
6/2/2014 11:08 AM | |
Posts: 73 Rating: (6) |
I had recently designed some test-jigs for testing of DI, DO and 2-wire AI. Based on these designs I had prepared the test-kits for my lab. Features of the test kits are as follows: Test Kit for DI / F-DI 1. Simulation of Standard / NAMUR-type switches. 2. Simulation of Wire-breaks / Short-circuit to study response of program under such conditions. Test Kit for DO / F-DO 1. Provision to test potential-free (dry) and wetted contacts. 2. Simulation of Wire-breaks / Short-circuit to study response of program under such conditions. Test Kit for 2-wire AI / F-AI 1. Provision to simulate 4-20mA signals. 2. Simulation of Wire-breaks / Short-circuit to study response of program under such conditions. Hope this is helpful to others. AttachmentC:\Users\in125702\Pictures\Pictures.zip (104 Downloads) |
This contribution was helpful to3 thankful Users |
6/2/2014 1:33 PM |
|
Joined: 10/19/2012 Last visit: 4/17/2022 Posts: 315 Rating: (9) |
Good effort & thanks for sharing. |