3/20/2023 9:12 PM | |
Joined: 3/5/2022 Last visit: 7/16/2023 Posts: 4 Rating: (0) |
I have a sinamics inverter G120C input voltage 380-480V and a motor with 440V closure.
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/21/2023 11:04:20New subject after splitting |
|
3/21/2023 12:11 PM | |
Joined: 3/27/2008 Last visit: 4/24/2024 Posts: 1097 Rating: (137)
|
This is fine, asynchronous industrial motors produce rated power and speed over a wide range of Voltage inputs, 380V to 400V , +/- 10% would be typical. Tractor |
Tractor |
|
3/21/2023 4:53 PM | |
Joined: 10/11/2006 Last visit: 4/24/2024 Posts: 5823 Rating: (789)
|
Hello Laraaa, See following application example for details explaining field-weakening operation. https://support.industry.siemens.com/cs/ww/en/view/25338130 If your motor and drive still meets the applicative demands torque/current, speed, etc., you can go with field-weakening. Otherwise you can use PISCEAN`s recommendation. |
With best regards, |
|
Follow us on