9/18/2016 6:50 PM | |
Joined: 3/28/2015 Last visit: 6/18/2022 Posts: 680 Rating:
|
Hello, Perhaps the following methods might help: Kindly find the attached file. AttachmentHow to setup Teamviewer VPN.pdf (71 Downloads) |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to
4 thankful Users |
9/18/2016 9:29 PM | |
Posts: 5225 Rating:
|
Friend Mohamed Ibrahim.. hope you are doing well. The PDF you have added - |
9/18/2016 9:41 PM | |
Joined: 3/28/2015 Last visit: 6/18/2022 Posts: 680 Rating:
|
Hello,
Good day to you This PDF explain a general procedure and can be applied to Simatic Manager and TIA Portal |
Eng.Mohamed Ibrahim |
|
9/19/2016 8:57 PM | |
Joined: 3/28/2015 Last visit: 6/18/2022 Posts: 680 Rating:
|
Hello William,
Realy, Iam not tested this procedure with TIA Portal But,we have many colleagues performed it and successed. They advise us with the following points: 1-Turn off firewall on both PC'S 2-Turn off antivirus on both PC'S 3-Follow the procedure as in the attached file. 4-Add a route to the PLC on the PG 5-Accessible nodes in TIA Portal not possible with VPN 6-Connect directly through IP address. AttachmentHow to setup Teamviewer VPN.pdf (48 Downloads) |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to
2 thankful Users |
9/19/2016 9:15 PM | |
Joined: 1/21/2016 Last visit: 6/28/2022 Posts: 83 Rating:
|
dear Murof the same ip are local ip but the public ip will be different should it make a problem ? Secure Remote Access to SIMATIC Stations via Internet and UMTS Attachment109476153_Remote_Panels_VPN_DOKU_en.pdf (51 Downloads) |
Last edited by: amrelhajali at: 9/19/2016 9:18:57 PMLast edited by: amrelhajali at: 9/19/2016 9:22:37 PMAmr Ali |
|
3/24/2022 1:46 PM | |
Joined: 8/3/2021 Last visit: 6/28/2022 Posts: 25 Rating:
|
Thank you all for the help on this issue. I have edited PDF and explained couple things which were confusing in Original PDF (liek what IP to use, and how to connect using TIA). I have tested with other types of PLCs and it worked as well. Once again thank you all! Edit: route add (IP of PLC) mask 255.255.255.255 (IP of Partner TeamViewer IP) metric 1 Forgot to add this explanation to original reply. AttachmentPLC Programming Remotely.pdf (19 Downloads) |
Last edited by: DonatasSM at: 04/13/2022 22:52:57 |
|
This contribution was helpful to
3 thankful Users |
Follow us on