5/14/2014 4:24 PM | |
Joined: 1/21/2013 Last visit: 10/8/2024 Posts: 4620 Rating: (708) |
HelloShailesh, If I understand correctly, you would like to send the PLC program in the HMI memory card? right? |
5/14/2014 4:47 PM | |
Joined: 5/28/2008 Last visit: 10/12/2024 Posts: 4515 Rating: (839)
|
Hello, You will need to use Bus Connectors with PG sockets for both PLC and OP. If you connected your PC / PG on the profibus network ans set the PC/PG ineterface correctly then you will be able to upload or download the PLC program by connecting the PC adapter or Profibus cable (in case of using Simatic PG) to the bus connector of Simatic Panel. And please note that old type of PC adapters "6ES7972-0CB20-0XA0" supports working with profibus networks up to 1.5Mbps baud. Which means if baud rate setting is higher than 1.5Mbps, it will not work. New PC adapters "6GK1571-0BA00-0AA0" supports up to 12 Mbps. Hope this helps.
|
Ayman Elotaify |
|
This contribution was helpful to1 thankful Users |
5/14/2014 7:51 PM | |
Posts: 784 Rating: (52) |
?
|
5/14/2014 8:26 PM | |
Joined: 10/24/2011 Last visit: 3/9/2023 Posts: 257 Rating: (1) |
HiAyman Elotaify, Thanks for quick reply. Then how I am able to see program blocks online in Accesible node? And I told already, in panel there is no CPU present. Only HMI and IM151-3 DP card in present.. Then How is program running? And In harware configuration, IM 153-1 DP (remote I/O card) is commuicating with HMI.(As there is no CPU in between). Is there any other way for this? How it had been done. Thanks, Shailesh |
5/17/2014 9:14 AM | |
Joined: 10/24/2011 Last visit: 3/9/2023 Posts: 257 Rating: (1) |
Hi Vipz, Ohhhk.. Is this setup freely available on forum? Or I need purchase it? Thanks, Shailesh
|
Follow us on