5/21/2011 10:55 AM | |
Posts: 947 Rating: (45) |
Hello josemiall May be should update firmware and driver for adapter.
see Installation of the PC Adapter USB/USB Prommer Driver with STEP7 V5.5http://support.automation.siemens.com/WW/view/en/44914284 Have you tried reinstalling the drivers forPC adapter USBindicate search the driver on the installation disk Step7, in the folder where you installed STEP7. May be step7 5.5 include new driver? as variant - install XP-mode and SIMATIC PC Adapter USB Software V2.0. My colleagues argue that it works |
Last edited by: gre_m at: 5/21/2011 2:03 PMLast edited by: gre_m at: 5/21/2011 11:13 AM |
|
8/6/2014 11:00 PM | |
Joined: 5/12/2011 Last visit: 4/24/2024 Posts: 6 Rating: (1) |
If you just installed Step7 manager, then just plug the adaptor to PLC and to your computer, the USB will appear automatically in the list of local connections if you don't have PLC you can connect 24vdc to the addaptor directly using the adaptor pin assignment sheet in this manual: |
2/19/2021 11:58 AM | |
Posts: 2 Rating: (0) |
USB MPI adaptor doesn't install in Simatic v 5.5 |
2/19/2021 2:41 PM | |
Joined: 9/21/2012 Last visit: 5/27/2024 Posts: 3952 Rating: (446) |
Did you plug in the USB A2 to the computer and PLC, both? |