10/13/2017 2:36 PM | |
Joined: 3/25/2015 Last visit: 10/30/2023 Posts: 94 Rating: (1) |
Dear Expert I'm commissioning NCU 710.3B SW4.5_SP4, During safety integration commissioning, there has Adapt SI Encoder softkey mentioned in user manual 9.2 Procedure when commissioning the drive for the first time I just finish all I can do in Siumerik Operate 4.5 through VNC view, if I de-active SI function, $MA_SAFE_FUNCTION_ENABLE = 0 and p9501 =0, everything was OK, the motor can be moved freely.( i use 1FK7 motor with 1-encoder system),
But if I active SI function, $MA_SAFE_FUNCTION_ENABLE=43H, p9501=43H, then I perform Active driver start-up->deactivate driver start-up->Copy SI->Confirm SI, then there is no alarm in VNC viewer. But once I press traverse key in HT8, alarm 201711 with code 3 appear, according to alarm description, it seems I need assign safety encoder. so I carefully check the manual, and found there has one step can not procedure by Copy SI, the manual said that I need press 'Adapt SI encoder' softkey in HMI advance, I running the HMI advance 7.3, but I still can't found this "Adapt HMI" softkey. Can anyone give me some instruction how to access this softkey?
NCU 710.3B with SW4.5 SP4
SINAMICS BOOKSIZE COLDPALTE10KW SLM
SINAMICS BOOKSIZE COLDPALTE 5A DMM
1FK7-xxxx-1RB0 motor with absolute encoder
HMI advance 7.3 running on windowsXP |
Last edited by: Nicholas2077 at: 10/13/2017 2:41:37 PMLast edited by: Jen_Moderator at: 10/16/2017 9:44:25 AMInserted right link and edited text for better reading. |
|