12/11/2015 8:40 AM | |
Posts: 87 Rating: (1) |
Hello Duris! New idea! May be I can use CP341 with connection half-duplex RS422 and in Layer1 - ASCIIdriver for this??? |
12/11/2015 9:49 AM | |
Posts: 87 Rating: (1) |
Yes of cause I too doubt......speed of CP its 115kbit, this is much less than the speed of XY2 ((((( and for two coordinate need two CP....( May be can I use external devices(high speed and ASCII) with Ethernet and communicate from S7 to him?.... something like this MGate 5105-MB-EIP Series this have 921.6 kbps ....I'm depressed this device wor with Modbus protocols....not have access to low level... |
Last edited by: andrewF at: 12/11/2015 10:00:16 AMLast edited by: andrewF at: 12/11/2015 12:08:49 PM |
|
1/12/2016 12:29 PM | |
Posts: 1 Rating: (0) |
May be this is a solution for you: http://halaser.eu/e1701.php This controller can be accessed via USB serial interface or via Ethernet and you can send more or less simple ASCII-commands to it in order to let the controller convert it to legal XY2-100 signals. |
1/13/2016 11:26 AM | |
Posts: 87 Rating: (1) |
This consturction based at http://beagleboard.org/BLACK and now I think about this way: construct own controller based in Arduino or other similar controller...... |
Follow us on