8/4/2018 9:24 PM | |
Joined: 5/23/2018 Last visit: 4/28/2022 Posts: 2 Rating: (0) |
hi everybody i have profibus DP communication problem when i replace sinamics g120 CU 240s-dp with cu240e-2dp one. i have replaced the cu in hardware configuration for CPU 417-5 H PN/DP_1 then i used the same telegram 352 which has used with CU 240s-dp and downloaded in plc but here LED indications in cu240e-2dp _____________________________ | RDY | BF | |_____________|______________ _| | green on/off | red flashing | (slow) |_____________|_______________.| and there is Alarm A1920 in diagnostic however when i open HW Config in simatic manager online , there is no any fault on cu240e-2dp icon on the bus also i uploaded cu parameters using starter v5.1. it will be found in attachment by the way i have configured the drive first on profibus telegram 352 before making HW configuration for cu240E-2DP on PLC ,i don't know , Is there a problem with that ? Coz in Micromaster440 all what i used to do is to assign p0918 for address, p1000, and p700 for Setpoint and command sources and put leave standard telegram in drive and changes it by PLC . could anyone help me in this problem , i would be very thankful? AttachmentCU240E-2DP.zip (74 Downloads) |
Last edited by: sin man at: 8/8/2018 10:27:15 AMLast edited by: sin man at: 8/8/2018 10:31:50 AMLast edited by: sin man at: 8/8/2018 10:33:48 AMLast edited by: sin man at: 8/8/2018 10:39:01 AM |
|