5/3/2008 1:20 PM | |
Posts: 3 Rating: (1) |
Dear All, In FI-01 wrote that the separation between LU01 and XPS sensor could be up to 365m with low capacitance coaxial cable RG62-A/U. But there was not mentioned anything about the capacitance and its value. Though, I searched for the cable and there was so many manufacturer which produce this cable, but specifications are different. So, I need advise in this regard. Attached you will findspecification from Fucol (cable manufacturer) which we are going to buy cable from them. Please kindly inspect the attachedspecification and advise if it could be suit for our purpose in maximum range of 300m or not. ( If not, please advise for the details of RG62-A/U and how to choose it.)
Your prompt reply would be highly appreciated. Best Regards, Hamed AttachmentRG62 AU.pdf (379 Downloads) |
Follow us on