19.10.2022 13:50 | |
Beigetreten: 05.10.2022 Letzter Bes: 12.04.2024 Beiträge: 2 Bewertung: (0) |
ElonksuM_SN_BNHi ElinksuM_SN_BN, thanks for your response!
Because if there is not I would not be able to download it using openness and would need to trigger it manually? |
Zuletzt bearbeitet von: michael!1234 am: 10/19/2022 13:51:19 |
|
20.10.2022 03:52 | |
Beigetreten: 19.06.2017 Letzter Bes: 26.04.2024 Beiträge: 7957 Bewertung: (162) |
Hi michael!1234, welcome to the Technical Forum! When creating your next topic, please keep in mind that there is a German and an international forum and try to discuss your question in the appropriate language. Since this is an international community, here is the translation of your post:
Best regards, |
My Forum is the place to personalize your profile, |
|
Folgen Sie uns auf