11.11.2017 03:39 | |
Beigetreten: 14.04.2006 Letzter Bes: 26.08.2024 Beiträge: 75 Bewertung: (2) |
Maybe our German collages can help: Hello Everyone, We are using PCS7/Batch V8.2, and are struggling to get the simple feature of auto-archiving of closed batches to a directory to work. If i test the connection to the directory for archiving from the BCC settings, (eg. \\ALLES1\ARCHIVING) from ES1, our recipe editing PC, the connection is fine. But if i test it from the other clients, i get the error message SIMATIC BATCH: CONTROL CENTRE DIRECTORY "\\CLIENT3\ARCHIVING" DOES NOT EXIST OR ACCESS IS DENIED. LOGON FAILURE: UNKNOWN USER NAME OR BAD PASSWORD. Even if logged on as Administrator. The directory is shared, and 'Everyone' has read and write permission. If i am on another client, i can access the folder, and create and delete files, eg a text file, from windows explorer. Anyone any Idea. Feel free to answer in German. Many thanks. |
13.11.2017 08:34 | |
Beigetreten: 19.06.2017 Letzter Bes: 06.09.2024 Beiträge: 8175 Bewertung: (171) |
Closed cause question posted twice.
|
Folgen Sie uns auf