(0)| 5/2/2022 8:56 PM | |
|
Joined: 10/17/2007 Last visit: 1/16/2026 Posts: 4579 Rating:
|
Hi, Friend, I know you need help asap, But can you please post at least one picture--this time I need to see your E/R module front with power up, and when you try to run the drives.(you said you make enable and set 1 V to run the drive) Secondary I need your machine detail story--I cannot guess you have a running machine? or you are making machine commissioning or start up. also you need to show--how are drives controlled by---?? CNC system? or PLC?? I attached page of 611A (I guess you have 611A) feed drive error list as your REF. PS: can you please open the 1st drive DC bus cover to see if the DC bus connecting --good? also test DC voltage from there. AttachmentFeed_drive_Error_list.pdf (1854 Downloads) |
Last edited by: nulizhang at: 05/02/2022 21:01:06If you like my comments please |
|
Follow us on