(0)| 1/22/2025 1:55 PM | |
|
Joined: 7/9/2015 Last visit: 1/15/2026 Posts: 4496 Rating:
|
Hi, yes this is possible because Memory Card contains all Data for PLC to run (Software + Hardware). If you change MC it could be, that PLC has to set to factory settings. If PLC is configured with protect confidential PLC data you must delete it like this here: Assign password via SIMATIC Memory Card Regards, Towome |
Last edited by: Towome at: 01/22/2025 13:57:51
|
|
| 1/22/2025 3:05 PM | |
|
Joined: 2/12/2024 Last visit: 1/6/2026 Posts: 12 Rating:
|
Hi Towome, Thanks for replying! If I set it to the factory setting, does it affect the old MC? My idea is if I am done with my test which is to download the new MC with the new program, I can put back the old memory which is the old program still working the same as before I replaced the MC. My colleague has experience in MC which has a password and after trying to put back the MC, the program is invalid. I don't want that to happen :) Regards, Kelvin
|
| 2/22/2025 6:50 PM | |
|
Joined: 2/5/2025 Last visit: 6/14/2025 Posts: 2 Rating:
|
All informations are deleted in the memory card when you are reset. |
| 2/24/2025 10:26 AM | |
|
Joined: 7/9/2015 Last visit: 1/15/2026 Posts: 4496 Rating:
|
Hi, thanks for your feedback - for this topic this FAQ could be also interesting for you: Download project data into the S7-1200/S7-1500 CPU without TIA PortalRegards, Towome |
|
|
|
Follow us on