3/19/2021 9:22 AM | |
Posts: 2 Rating: (0) |
I also have the same problem as above but the software requested is different, that a warning appears "Missing Software Packages --- The Following Objects in this project cannot be processed as the appropriate software packages have not been installed: Dcc_Container --- SinamicsPUType1. 0 ". and on the accessible node all projects have the question mark logo, and I can't go online. Can someone help me? why is this happening? thank you very much . ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/19/2021 12:21:01New subject after splitting |
|
3/20/2021 3:43 AM | |
Posts: 2 Rating: (0) |
Thanks for your advice Sir, yes Simatic CFC V9.0+Sp3+Upd1 is Installed |
Follow us on