(1)| 4/12/2021 9:38 AM | |
|
Joined: 3/1/2016 Last visit: 9/6/2022 Posts: 25 Rating:
|
Ensure that the latest firmware version of 'FC360 Desktop Editor 2.0' is installed on the PC. Download the latest Version from the getting started page.Link 1. Connect the PC to the panel. 2. Set Windows firewall.(Manual for firewall settings) 3. Enter access level 3 password to log into level 3 on the panel. 4. Open 'FC360 Desktop Editor 2.0'. 5. Click 'Update Firmware'. ->The panel starts to update the firmware.-> A successful message is indicated. Otherwise, a failure message is indicated. 6. Check the version on the panel. See menu item 'About. 7. Disconnect the PC from the panel. |
Last edited by: kai_moritz at: 04/12/2021 09:50:50Last edited by: Jen_Moderator at: 04/12/2021 13:06:13Optimized link. Edited text for better reading. Last edited by: kai_moritz at: 04/28/2021 13:28:24 |
|
Follow us on