2/4/2020 4:39 PM | |
Joined: 9/9/2012 Last visit: 7/16/2024 Posts: 48 Rating: (0) |
Hello, We have a PAC3200 and We want to show values in HMI, check if we are inside normal values, perhaps store data,.... I have followed the manual: Entry ID: 109739102, Entry date: 04/18/2018 ------ And downloaded the program with example, but when I try to generate objects, it gives me an error. Invalid configuration for energy object: Energy_object_1.,2/4/2020,4:22:28 PM I check that is configured license for <5 energy objects, in the energy object there is nothing in red, periods are configured,.. everything seems OK.... but error when generating it. But summarizing, What I want is nothing special,.. see values, store data,.... I don't need if I need the complete energy suite for my purpose or just with a simple communication I can achieve my goal. I also saw that there is another option for communication,... SIMATIC S7-1500 Block for Connecting Modbus TCP Devices to Energy Suite V15 Would be this last one a better option for simple purposes? |
There are 10 types of people in this world, those who understand binary and those who dont. |
|
Follow us on