4/13/2021 8:04 AM | |
Joined: 9/30/2016 Last visit: 7/11/2024 Posts: 914 Rating:
|
Please also see the attached screenshots. I have a metercounter that is not counting. I can see on the faceplate that it is not enabled. When I check the PLC logic I can see that in order to enable the block I need to have the line running. But even when the line is running and DB4044:DBX34.0 is active in network 2 it is NOT active in network 3. I is also not active (as DB4044,D34.0) on the faceplate. How is this possible and how do I make the bit active in the places where it is used? AttachmentFC2 MT.zip (177 Downloads) |
Follow us on