4/16/2021 1:53 PM | |
Joined: 2/15/2021 Last visit: 4/14/2022 Posts: 14 Rating: (0) |
Hi Dimsenio, You seem to have some experience with the V20. I have a project where I use only 1 speed but I want to run in reverse aswell. Do you have the possibility to tell me if it´s possible to change the rotation with the logo without any bus communication? I will have two limit switches. One in each end for the movement. I will program the logo to decide the rotation depending on wich switch is active. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/19/2021 07:39:04New subject after splitting |
|
4/19/2021 7:57 AM | |
Joined: 6/19/2019 Last visit: 9/5/2024 Posts: 697 Rating: (73) |
Hello, Yes you can change rotation without bus communication, you need to connect wires and change settings for you your V20. See P700 to 2bit (Terminal) P701 to bit 1 (ON) P702 (second terminal) program to bit 2 (ON reverse) See video |
Last edited by: Mr.V at: 04/19/2021 08:08:01Last edited by: Mr.V at: 04/19/2021 08:12:02Last edited by: Jen_Moderator at: 04/19/2021 12:31:05Embedded video. |
|
This contribution was helpful to1 thankful Users |
Follow us on