4/21/2021 3:23 PM | |
Joined: 1/4/2007 Last visit: 9/2/2024 Posts: 1142 Rating:
|
Hello AV1234, Well, I would like to take a look to your TIA Porject. But before I did this, I played a little bit with the existing Ready-for-Use projects from the Internet. And indeed, it’s not so easy to create a TIA project with S7-1200, the WP321 module and the HMI-panel. But the issues, which I had, wasn’t the Siwarex module, but the handling in TIA Portal! It takes a while, but it was possible for me, to create such a TIA Portal project. (It’s for TIA V16.) See my TIA project attached, please. (I had to zip this TIA project to upload the file.) At the end, I didn’t take a look to your TIA project. Best regards Siwarexi
AttachmentS7-1200_WP321_KTP700Basic.zip (887 Downloads) |
Follow us on