7/4/2017 9:27 AM | |
Joined: 4/28/2015 Last visit: 12/20/2023 Posts: 42 Rating: (1) |
hi, find attachment Excel report script,based on trigger. Attachmentexcel bharat fogre.txt (1431 Downloads) |
This contribution was helpful to3 thankful Users |
11/15/2017 8:07 AM | |
Joined: 5/9/2017 Last visit: 4/30/2024 Posts: 1 Rating: (0) |
Can u please share the .pdl of your project, where you have used the above script.. |
11/23/2017 5:48 AM | |
Joined: 5/22/2010 Last visit: 3/26/2024 Posts: 97 Rating: (2) |
Hello Niksss, Can you please explain what is your requirement. Regards Manish |
5/18/2019 7:42 AM | |
Joined: 8/19/2017 Last visit: 4/28/2024 Posts: 79 Rating: (3) |
Dear Georg Berghof You said that it is not possible to connect Excel to Wincc directly, but from wincc help under interfaces>OPC - Open connectivity>Wincc OPC DA server>Example of OPS DA Connections>Wincc - Microsoft Excel connection, there is an example of connecting the wincc directly to the Excel. I'm working on this, but I get an error that I attached below. If anyone used this example, I'll appreciate any help. And this link opens with the help button of the error. thanks in advance. |
Last edited by: Soroosh.v at: 05/18/2019 07:47:12 |
|
5/2/2021 12:25 AM | |
Joined: 9/27/2006 Last visit: 5/9/2024 Posts: 12257 Rating: (2666) |
Hello Omkris; The thread is over 2 years old, documents and links have evolved since then. You have been with us long enoug to know how to use the search box at the right of this page to locate the inofrmation you need on WinCC, no? Here are brief introductions to the options proposed by Mr. Berghof. - WinCC Basic Options V7.4 SP1: WebNavigator, DataMonitor, WebUX, Connectivity Pack https://support.industry.siemens.com/cs/gb/en/view/109746337 - Delivery Release SIMATIC Information Server 2014 SP3 https://support.industry.siemens.com/cs/gb/en/view/109750806 Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on