5/7/2021 3:59 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928)
|
Hi, You can use the remaining time from the timer (output sfc) and connect it to the Setpoint _AI value (actual input). The Setpoint must be of type Real and you can use it to set the time (TIME0). In the Actual Values you can see the time counting down. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
Follow us on