4/27/2021 9:02 PM | |
Joined: 2/23/2017 Last visit: 7/19/2024 Posts: 37 Rating:
|
Hi there, I'm almost there with a small project to control a 0..10V lamp via my LOGO. I have two push-buttons, UP and DOWN. Both should vary the light accordingly when pressed longer than 0.5 seconds and switch ON (for UP) and switch OFF (for DOWN) if pressed shortly (<0.5s). I've found most of this program in this forum so and I'm very thankful for it. Everything works as expected but the ON button. I can't find the way to make the light switch ON fully (value = 100) when pressed shortly. B011 is the block that sets the dim level (0=OFF ...100=full ON). A long press (> 0.5s) "DOWN" makes B011 decount slowly (good!). When I short press (<0.5s) "DOWN", blocks B001/B002/B007 reset B011 that will switch the light OFF. A long press of "UP" makes B011 count up and the light level rises slowly (good!). And now my problem: how do I make a short press of "UP" to set B011 to 100? B008's output (="set light to 100") is unconnected because I don't know to what or where I should connect it.... Thanks for any suggestion. BR Roger AttachmentAnalog Light Control With Two Buttons.zip (321 Downloads) |
Last edited by: flotul at: 04/27/2021 21:04:09Last edited by: flotul at: 04/27/2021 21:07:14 |
|
4/29/2021 8:15 AM | |
Joined: 6/19/2019 Last visit: 7/10/2024 Posts: 697 Rating:
|
Hello, For short press i will do latch relay to count up and it count until 100 AttachmentAnalog Light Control With Two Buttons.zip (307 Downloads) |
4/29/2021 1:23 PM | |
Joined: 2/22/2008 Last visit: 6/12/2024 Posts: 2698 Rating:
|
Maybe an analog counter would be a better solution for a dimmer, see attachment. The speed for counting up or down may be slowly in a simulation, try it in a Logo controller. If 0.01s is not fast enough in real time, then change maximum value from 1000 to e.g.100 and insert an amplifier with gain=10 between dimmer value and AQ1. Regards, Scorp AttachmentDimmer1.zip (319 Downloads) |
4/29/2021 2:09 PM | |
Joined: 2/23/2017 Last visit: 7/19/2024 Posts: 37 Rating:
|
Thank you Mr.V, Your solution works and it is a good option. |
5/11/2021 2:35 PM | |
Joined: 2/23/2017 Last visit: 7/19/2024 Posts: 37 Rating:
|
Thanks Scorp, I'll give it a try asap ;-) |
Follow us on