6/4/2010 7:32 AM | |
Joined: 3/24/2009 Last visit: 6/20/2023 Posts: 535 Rating: (112) |
Dear sidou1, if you want to get information about channel-faults, you have to read the system status list of the module via the SFC51. In the attachment you find a STL-source, which you also can find in the help of the SFC51. Best regards, yy1 Find additional info on the diagnostic data in this link. AttachmentOB82_sfc51.zip (699 Downloads) |
Last edited by: yy1 at: 6/4/2010 9:44 AMAdditional link |
|
This contribution was helpful to3 thankful Users |
6/28/2011 4:03 PM | |
Posts: 35 Rating: (0) |
here it is as an attachement my program. Use this program and configurate for me only a DIAGNOSTIC fault of one channel of the first analogique input. this fault must be shown as an alarm in my MP 270.
Attachmentcompresseur cooper_Co_.zip (420 Downloads) |
6/28/2011 4:22 PM | |
Posts: 270 Rating: (53) |
Dear sidou1, I saw your problemhere on the forumand I would also like to help you. I personaly think, that this topic might help you, it might not seem easy at first glance, but once you get into it, I am sure it will work out really great for you. Anyway, have a nice day. Best regards, MM1234 P.S. I hope your technical problem will work outtoo, unfortunately I don't seem to see into that very well. |
6/28/2011 5:30 PM | |
Joined: 10/7/2005 Last visit: 4/26/2024 Posts: 3004 Rating: (1046)
|
Hello sidou1 now that we've established that you use a Siemens HMI, you could of course simply use the inbuilt Report System Error functionality, just to mention it. |
Cheers |
|
Follow us on