5/31/2021 2:08 PM | |
Joined: 4/24/2006 Last visit: 6/17/2024 Posts: 8683 Rating:
|
Hello, Have you seen the following links: How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet? Why can you not transfer the HMI configuration to the panel? Is the panel connected to PC? (Or are there switches in between?) (Try to connect HMI panel to PC) Best regards, Wizard |
5/31/2021 2:11 PM | |
Joined: 2/17/2020 Last visit: 6/14/2024 Posts: 1010 Rating:
|
Hi m19star, I consider that the following FAQ is very useful for this type of communication problems with HMI panels: Why can you not transfer the HMI configuration to the panel? I hope it helps.
|
A rating will be well appreciated. |
|
5/31/2021 2:15 PM | |
Joined: 2/17/2020 Last visit: 6/14/2024 Posts: 1010 Rating:
|
It seems that Wizard and I wrote at the same time haha The issue of intermediate elements is relevant as well (such as switches), as they could be the real problem. Also, disabling firewall and antivirus on the PC could help, as it sometimes blocks communication.
|
A rating will be well appreciated. |
|
This contribution was helpful to
1 thankful Users |
Follow us on