6/3/2021 9:42 PM | |
Joined: 5/20/2021 Last visit: 4/8/2022 Posts: 55 Rating:
|
Hi, im trying to control peristaltic pump(motor speed) using 4-20mA incoming signal. first mode: just using cuser from plc to increase and decrease the pump( its working good). second mode: using push button (set remote start/stop) I1 but its runing by 0.1 % step . i would like to run the pump when i activate this button without step(contiunous runnig) and limited like for 80%(stop automatically). i use logo 8.3. thanks. Attachmenttest1_peristaltic pump.zip (261 Downloads) |
6/3/2021 10:03 PM | |
Joined: 12/18/2014 Last visit: 7/18/2024 Posts: 33374 Rating:
|
You want not learn. You make also a new topic for the same problem. control speed peristaltic pum flex pro serie A2V |
6/4/2021 11:31 AM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating:
|
The second thread with the subject control speed peristaltic pum flex pro serie A2V is published within the conference LOGO! - Projects. Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on