6/3/2021 6:24 AM | |
Joined: 3/24/2018 Last visit: 5/5/2024 Posts: 236 Rating: (1) |
Hi,
Dear ChristophD, Iam not able to select COM1 and bit rate inPG/PC settings as in the picture. I installed teleservice V 6.1 SP5( Successfully installed)support windows7 COM1 is o.k Window 7 Sp1 64 bit Simatic manager v5.6 sp2 is o.k Ts adapter not work when use it to connect with CPU S7-300 "connection can't be estabilshed' Thank you in advance. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/04/2021 10:11:21New subject after splitting Last edited by: Pepsi Cola at: 06/04/2021 17:28:07Last edited by: Pepsi Cola at: 06/04/2021 21:33:23Last edited by: Pepsi Cola at: 06/05/2021 07:45:25 |
|
6/7/2021 2:06 PM | |
Joined: 5/12/2006 Last visit: 8/7/2024 Posts: 22337 Rating: (3000)
|
which settings used in the tab Local modem? |
6/7/2021 5:38 PM | |
Joined: 3/24/2018 Last visit: 5/5/2024 Posts: 236 Rating: (1) |
Hi, The setting of the local modem as in the attached photo. |
Last edited by: Pepsi Cola at: 06/07/2021 18:11:58 |
|
6/7/2021 6:16 PM | |
Joined: 3/24/2018 Last visit: 5/5/2024 Posts: 236 Rating: (1) |
HI, Photo 2 |
6/7/2021 6:21 PM | |
Joined: 3/24/2018 Last visit: 5/5/2024 Posts: 236 Rating: (1) |
HI, Photo 3 |
Follow us on