6/16/2021 12:39 PM | |
Joined: 6/10/2021 Last visit: 4/7/2023 Posts: 10 Rating: (0) |
I try to operating Get the following result |
6/16/2021 12:43 PM | |
Joined: 5/12/2006 Last visit: 8/7/2024 Posts: 22337 Rating: (3000)
|
do you have line filter / AIM? |
6/16/2021 12:45 PM | |
Joined: 6/10/2021 Last visit: 4/7/2023 Posts: 10 Rating: (0) |
No My system only breaker>SLM>SMM |
6/16/2021 12:51 PM | |
Joined: 5/12/2006 Last visit: 8/7/2024 Posts: 22337 Rating: (3000)
|
wrong wired |
6/16/2021 12:55 PM | |
Joined: 6/10/2021 Last visit: 4/7/2023 Posts: 10 Rating: (0) |
The line filter and line reactor necessary? |
6/16/2021 12:55 PM | |
Joined: 5/12/2006 Last visit: 8/7/2024 Posts: 22337 Rating: (3000)
|
if you don't want such faults about the phases, yes |
6/16/2021 12:59 PM | |
Joined: 6/10/2021 Last visit: 4/7/2023 Posts: 10 Rating: (0) |
If I don't care the phases. The starter allow to ignore the faults? |
6/16/2021 1:00 PM | |
Joined: 5/12/2006 Last visit: 8/7/2024 Posts: 22337 Rating: (3000)
|
no is not possible to ignore it |
Follow us on