6/18/2021 7:18 PM | |
Joined: 5/20/2021 Last visit: 4/8/2022 Posts: 55 Rating:
|
Hi, my goal is to distribute water to patients using 2 drums (preffilled with water) with one pump.the principles is that the pump work in 2 senses of rotation( i find a solution that i connect an output from the Logo Q1 to the Input on the pump so i can switch the direction of rotation with my switch button). i try to do step 1(file etape1) in this project that i control the level of one drum by pressure transducer and its working.now is there any help or suggestion to do my scenario in this project: -the pump will turn on, untill the the first drum will be level low ( valve 1a and 1b are openend; 2a and 2b closed) -after that, the pump reverse rotation and trun on till the second drum will be low level ( valve 2a and 2b are openend; 1a and 1b closed). the drum dimension (34inch*24inch) level low : 4inch valve types: proportionnel valve 2-10V (analog output AQ) thanks Attachmentetape1.zip (256 Downloads) |
Last edited by: bessem87 at: 06/18/2021 19:18:38 |
|
6/18/2021 9:55 PM | |
Joined: 12/18/2014 Last visit: 7/19/2024 Posts: 33376 Rating:
|
Sorry, but I can't understand you. Why make you a new topic? You have already make a topic for your problem: reverse rotation of pump with logo |
6/21/2021 3:31 PM | |
Joined: 12/18/2014 Last visit: 7/19/2024 Posts: 33376 Rating:
|
And why make you a new topic? I can't understand you. |
6/22/2021 7:56 AM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating:
|
Closed cause question posted twice. The second thread with the subject reverse rotation of pump with logo is published within the conference LOGO! - Projects. Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on