6/23/2021 10:13 AM | |
Posts: 4 Rating: (1) |
I have just recived feedback from siemens. See: https://support.industry.siemens.com/cs/ww/en/view/109798574 |
Last edited by: Jen_Moderator at: 06/23/2021 13:48:45Optimized link. |
|
This contribution was helpful to1 thankful Users |
6/26/2021 6:54 PM | |
Joined: 3/4/2006 Last visit: 4/19/2024 Posts: 73 Rating: (3) |
Thank you. I’ll be trying that next week. |
6/30/2021 7:42 PM | |
Joined: 3/4/2006 Last visit: 4/19/2024 Posts: 73 Rating: (3) |
It is indeed working. I had to reinstall some of the HSPs as it indicated, and disable the integrity monitoring. |
7/1/2021 8:40 AM | |
Joined: 10/6/2011 Last visit: 4/16/2024 Posts: 5 Rating: (1) |
Hi, I had exactly the same problem and after a couple of days of emails with Siemens Support they sent me the link below to the S7-PM software but told me that it will need a licence if the functionality is used but at present they can't see the licence in the Mall. I have installed the software and the read-only problem has gone and I can now edit my project. As far as I can tell the functionality of the software hasn't been used in the project so I am not getting any licencing problems as yet. https://support.industry.siemens.com/cs/gb/en/view/109798411 Note the software is export restricted so you need to be approved to download. See link below if you are not. https://support.industry.siemens.com/cs/nl/en/view/109744535 Hope this helps |
Last edited by: Goody at: 07/01/2021 08:43:14 |
|
This contribution was helpful to2 thankful Users |
Follow us on