7/14/2021 3:49 AM | |
Joined: 9/9/2015 Last visit: 10/10/2024 Posts: 728 Rating: (278) |
Hi EBM, Entire compilation does not lead to a entire plc download. To download PLC changes, the timestamp should be the same and most of the DB structure in offline and online should be matching. you can do a backup before entire compilation, if a full download is needed after entire compilation, you can restore back your as project. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
Follow us on