Industry Online Support
Technical Forum
8/2/2021 4:44 PM | |
Posts: 2 Rating: (0) |
Good afternoon. Please help in solving the problem: I have an old MOBY I identification system on my equipment. We connect it to the S7-317F controller built into the NCU module (6FC5371-0AA30-0AB0) via the ET200M module (6ES7153-4AA01-0XB0) PROFINET via the ASM475 module (6GT2002-0GA10). Description of the problem: After the Hardware and program blocks are loaded into the controller, the ERR1 and ERR2 LEDs on the ASM modules blink (1 blink per 3 sec.) In the DB block for controlling ASM modules, errors FC_Error - B # 16 # 08 and BUS_Error - B # 16 # 8093 To program the MOBY I, I use the FC45 block. Can you please tell me if it is possible to connect ASM475 modules to the controller via ET200M (Profinet)? If so, where is the error in the parameterization of the modules? Can FC45 be used? Where can I download the FB55 block? Following the link on your website http://support.automation.siemens.com/WW/view/en/61199127 it is not available to me (error) Attached are screenshots with system configuration and program blocks for controlling ASM modules.
AttachmentDoc1.pdf (727 Downloads) |
Follow us on