8/6/2021 10:14 PM |
|
Joined: 9/21/2012 Last visit: 5/8/2024 Posts: 3937 Rating: (444) |
You're not making any sense.... |
8/6/2021 10:26 PM | |
Joined: 9/27/2006 Last visit: 5/8/2024 Posts: 12257 Rating: (2666) |
Hello tigranes; In the off chance that you are asking us what software you need to program a S7-1200 PLC, you need a Step 7 Basic installation, v16 for example. If you want to program a S7-1200, plus a S7-1500, S7-300 or S7-400, you would need Step 7 Professional version. https://support.industry.siemens.com/cs/ww/en/view/109771628 If that is not the answer you were seeking, maybe you should rephrase the question in terms we might understand. Hope this helps, |
This contribution was helpful to1 thankful Users |
8/6/2021 10:43 PM | |
Joined: 9/21/2012 Last visit: 5/8/2024 Posts: 3937 Rating: (444) |
I would like to add to Daniel's excellent answer, that you can find out the needed software and the minimum version from the product datasheet. |
This contribution was helpful to1 thankful Users |
8/6/2021 11:43 PM | |
Joined: 3/28/2015 Last visit: 5/4/2024 Posts: 721 Rating: (213) |
Hello, CPU 1212C, DC/DC/Relay, 8DI/6DO/2AIFirmware version 4.5 :Required software TIA Portal with STEP 7 V17 Basic or STEP 7 V17 Professional or higher. Firmware version 4.4 :Required software TIA Portal with STEP 7 V16 Basic or STEP 7 V16 Professional or higher. Firmware version 4.3 :Required software TIA Portal with STEP 7 V15.1 Basic or STEP 7 V15.1 Professional or higher. Firmware version 4.2 :Required software TIA Portal with STEP 7 V14 Basic or STEP 7 V14 Professional or higher. Firmware version 4.1 :Required software TIA Portal with STEP 7 V13 SP1 Basic or STEP 7 V13 SP1 Professional or higher. |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to1 thankful Users |
Follow us on