8/23/2021 1:47 PM | |
Joined: 12/18/2014 Last visit: 6/15/2024 Posts: 33197 Rating: (4105)
|
Can you please upload your LOGO! program and the LWE project as a ZIP file? |
8/23/2021 2:09 PM | |
Joined: 2/6/2021 Last visit: 2/14/2024 Posts: 5 Rating: (0) |
uploaded - thank you.
Attachmentsimple example.zip (135 Downloads) |
8/23/2021 2:23 PM | |
Joined: 12/18/2014 Last visit: 6/15/2024 Posts: 33197 Rating: (4105)
|
In the Parameter-VM-Mapping table use you parameters with the format DWord. The addressing in the LOGO! is byte oriented. A DWord included 32 bits or 4 Bytes or 2 words. If you use by the first DWord the address 2 then use you VB2 till VB5 for this. See you the overlapping? If you use for the first DWord the address 2 then is the logical address for the next DWord 6, not 3. AttachmentLOGO! Bit, Byte, Word and DWord.pdf (156 Downloads) |
8/23/2021 2:32 PM | |
Joined: 12/18/2014 Last visit: 6/15/2024 Posts: 33197 Rating: (4105)
|
That sounds good ... |
Follow us on