3/4/2009 10:34 AM | |
Posts: 10 Rating: (0) |
Hi! Remote-Host:161.53.71.219 Destination-Port:26862 Source-Port:RANDOM Remote-Host2:NONE Destination-Port2:26862 Source-Port2:RANDOM Server-Mode:MSC Server-Line:LL Server-Username:modem1 Server-Username2:NONE Dial-Up:GPRS System-Time:8265 Terminal-Mode:DISABLE Firmware-Version:V1.7.3 SIM-Status:SIM_ERROR Provider: NetID: APN: Quality:99 COM-Control:ALWAYS_ON COM-Baudrate:9600 COM-Format:8N1 It seems that PLC and modem are communicating because remote host, port or modem name parameters are the same as one specified in PLC. But still it SIMSTATE indicates SIM error and there is no APN eventough it is specified in the PLC. I also tried to make factory reset of MD720 but it is still the same. Now I don't what could be the cause for such a behavior? Should I suspect on the MD720 hardware or it is maybe problem in the communication between CPU and MD720. Please give me some advice. Many thanks Regards Alen Attachmentmd720_gprs_V0.zip (72 Downloads) |
3/4/2009 1:55 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello SIM card must be with a CSD service, PIN activated. (The PIN must not be deactivated!) regards |
Follow us on