9/13/2021 3:13 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating:
|
Hello, It seems like your flow is causing node-red to crash. If you delete the flows JSON-FIle inside of
And restart the IOT/Node-Red, you should be able to access the UI of node-red again. Then check which version of the Modbus Nodes are installed? -> "Manage Palette" This example recommends to use v4.1.1: to install it
BR |
Follow us on