9/8/2021 12:53 PM | |
Joined: 1/10/2019 Last visit: 6/7/2024 Posts: 3 Rating: (0) |
Dear Experts, Have connected to internet. Manage to download and install node-red-contribs-S7 and node-red-contribs-http. But nevertheless, I cannot installed node such as node-red-dashboard and many other nodes. Attached is the log view when fail to install. To add on, my colleagues with the same version of node red and node.js in their laptops are working fine with the installation. Looking forward to advices. Thanks Attachmentsubmit1.pdf (235 Downloads) |
Last edited by: AutoGen_4729356 at: 09/08/2021 13:16:27 |
|
9/15/2021 5:26 PM | |
Joined: 4/17/2018 Last visit: 5/8/2024 Posts: 86 Rating: (5) |
Hi, just to ask: Do you try to install the palette on the example image or do you use the IndustrialOS? |
Follow us on