9/4/2021 11:02 PM | |
Joined: 6/26/2021 Last visit: 4/11/2024 Posts: 3 Rating: (0) |
This topic is extremely important for me as I am using a library of FB's and consequently DB instances for motors, valves,.. I absolutely don't see any good future with Unified where everywhere Siemens is writing how the UDT approach just super great and how it makes less work in relation to Faceplates. Can you explain how I can connect my DB's for each valve, motor,... with a faceplate without useless workarounds and using UDT's... And now even the "change object references" is gone - this is back to 1998 ... ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/06/2021 12:13:27New subject after splitting |
|
9/5/2021 6:31 AM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
I have never used unified but it looks like it has multiplexing. |
Last edited by: Jen_Moderator at: 09/06/2021 12:15:21Embedded video. |
|
9/7/2021 10:06 AM | |
Joined: 2/13/2020 Last visit: 1/28/2023 Posts: 54 Rating: (10) |
This multiplexing only works if data is in an array which it is not since he wants connect an IDB to a faceplate. I don't see any good way to link it without fundemental change in how the program is set up in the PLC, either by using UDTs or by having one FB with the instances of each arrayed. |
Follow us on