10/2/2021 11:28 PM | |
Joined: 9/27/2006 Last visit: 6/27/2024 Posts: 12264 Rating: (2672) |
Hello Vorapob; There is an instruction in Ste 7 "STP" that can be used (and triggered via your HMI program) to place the CPU in STOP mode; it is availble in SCL, LAD and FBD: https://support.industry.siemens.com/cs/ww/en/view/109773506/94485540619 However there is no instruction available treturn the CPU in RUN, when it is in STOP mode. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 10/02/2021 23:29:26 |
|
10/3/2021 7:25 AM | |
Joined: 12/18/2014 Last visit: 6/27/2024 Posts: 33250 Rating: (4114) |
Take a look at this FAQ: How do you evaluate the "RUN / STOP" mode of the CPU via an HMI operator panel?Attached a screen video of my test with a real S7-1212C and a simulated KTP1200. AttachmentPLC mode (RUN_STOP) changed bei HMI.zip (414 Downloads) |
This contribution was helpful to2 thankful Users |
Follow us on