10/1/2021 8:09 AM | |
Joined: 9/4/2012 Last visit: 4/24/2024 Posts: 18 Rating: (0) |
Hello all. We have this issue now on 5 devices. All with the same HW: CPU 1515SP F - 6ES7 677-2SBx2-0xB0 We tried this solution but it does not solve the problem. Any updates? BR |
Last edited by: Jen_Moderator at: 10/01/2021 09:51:10Optimized link. |
|
10/5/2021 2:30 PM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hello MAZA1980 The cause could be the host controller drivers that are equipped with the bundle V2.6.2. The problem should be resolved with the bundles from V20.8. See also the information in the FAQ: Why does the Windows system time change when you perform a "cold start" on the SIMATIC ET 200SP Open Controller? With best regards |
Follow us on