10/7/2021 9:51 AM | |
Joined: 7/5/2018 Last visit: 2/22/2024 Posts: 19 Rating: (2) |
Hello RafaVidal, Please send a screenshot of the error shown. mui94 |
This contribution was helpful to1 thankful Users |
10/8/2021 7:37 AM | |
Joined: 6/19/2017 Last visit: 5/3/2024 Posts: 8006 Rating: (163) |
Hi RafaVidal, Please try to discuss your question in English language. This is an international community and we try to focus on one language. Posting in English will help you to get more response to your question. This is the translation of your question:
Regards, |
My Forum is the place to personalize your profile, |
|
10/8/2021 9:22 AM | |
Joined: 7/5/2018 Last visit: 2/22/2024 Posts: 19 Rating: (2) |
Hello Rafa, about the message that appears referring to the memory, even if it is not completely full, when you load your device, the equipment requires part of this memory to perform an internal compilation and then load the program itself. If the CPU does not have space in its memory for this compilation, this message appears. This is usually solved if you safely remove the memory card and with the help of a Field PG load the project directly onto it. As for the web server problem, I would recommend that you contact Siemens Technical Support. mui94 |
This contribution was helpful to1 thankful Users |
10/8/2021 10:14 AM | |
Joined: 8/14/2021 Last visit: 2/4/2024 Posts: 12 Rating: (0) |
Thanks Mui94, and sorry for send my message in spanish. Thanks. |
Follow us on