3/8/2009 12:36 PM | |
Posts: 103 Rating:
|
how are you all, |
Last edited by: ahmedmae94 at: 3/8/2009 1:16 PMLast edited by: ahmedmae94 at: 3/8/2009 12:48 PMLast edited by: ahmedmae94 at: 3/8/2009 12:46 PMLast edited by: ahmedmae94 at: 3/8/2009 12:43 PMLast edited by: ahmedmae94 at: 3/8/2009 12:40 PMLast edited by: ahmedmae94 at: 3/8/2009 12:38 PM |
|
3/10/2009 2:17 PM | |
Joined: 5/13/2008 Last visit: 12/18/2019 Posts: 836 Rating:
|
Hi ahmedmae94, I'm a bit confused about the assembly you like to get it started. If you use a S7-300 and a PC with WinCC flexible, wired by profibus, then there is no need for OPC. If you like to connect another application (e.g. Excel) to WinCC flexible, you can use OPC. If both is running on the same machine, you do it by COM (as J_Bell already told you). COM doesn't need any further adjustments, unlike DCOM. In that case, WinCC flexible would be an OPC-Server and Excel the OPC-Client. A more detailed description can be found here: http://support.automation.siemens.com/WW/view/en/18657078 |
mfG / Best regards |
|
3/10/2009 4:32 PM | |
Posts: 5822 Rating:
|
Hello, Roland is right, COM does not require any settings at all, it runs as soon as Windows is up and running. Best regards J_Bell |
3/15/2009 8:22 AM | |
Posts: 103 Rating:
|
thank you for your response |
Follow us on