10/26/2021 4:22 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi, Bit memory is a static variable and is reset when the SFC is downloaded with a full download (changes to default value), but value is retained until it's overwritten by another value or deleted from the SFC. The variable is called in the SFC instance. |
Last edited by: Oreca at: 10/26/2021 18:18:29If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on