Industry Online Support
Technical Forum
4/11/2008 6:05 PM | |
Posts: 32 Rating: (0) |
But, i need use a SINAMICS G110, no Micromaster, The limitation of slaves its in SINAMICS? So, i need use a PWM Control... If Posible. Best Regards. |
4/11/2008 6:07 PM | |
Posts: 32 Rating: (0) |
escuseme, im wrong, if posible, max 31 salves sinamics... |
3/18/2009 10:39 AM | |
Posts: 7 Rating: (0) |
Hi!, Is it possible to find an application/example for the PID pulse width modulation using the blocks FB41, 43 etc...? Thanks! |
3/18/2009 1:06 PM | |
Joined: 4/21/2006 Last visit: 9/23/2024 Posts: 510 Rating: (24) |
Closed: This thread is closed because the question was posted twice. The other thread you can find here: Application/example on the PID modulation with impulsion. |
Follow us on