11/15/2021 10:45 AM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating: (377)
|
Hi, thanks for you interest! 1) The OS : sudo is required when you are logged in as user and want to perform operations you need administrative priviledges for. sudo is not needed when you are logged in as root You don't need the OSS packages for anything. From a legal perspective we need to provide the used open source packages. That's what you can find in the .zip folder(s). 2) Node-RED We do not have an image V1.0.3. I guess you mean the Example Image V1.0.2. But this version of the Example Image, as well as the current release V1.1.1, does contain the GPIO nodes. There is no repository for Siemens nodes, but you can install the nodes available from node-red's webpage. Right, if you are installing another version of node-red the GPIO nodes won't be available, because node-red gets installed in different path when updating it. But there is a way to copy the GPIO nodes to the new location. 3) GPIO Usually the Arduino pins work. If you are using the Siemens I/O shield, it is required to set the jumper X82 to pins 1-2 (as described in the shields manual). This behavior sounds not as intended, maybe there is a short circuit anywhere? Does the potentiometer work on other devices? Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
11/22/2021 7:54 AM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating: (377)
|
Hi, this answers refers to 2) Node-RED only. The node-red version has nothing to do with the availability of the GPIO nodes. They are pre-installed only in the Example Image, not on the Industrial OS. You can use the Example Image on an SD card or the eMMc. Maybe it is more easy to run it on the SD card first to check the features, because you can simply re-write the image again if there is something going wrong. There is another description running it on the eMMc here. At first perform point 3.6 from the Industrial OS documentation (as you already mentioned) and the follw the eMMc document. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
11/28/2021 5:20 PM | |
Joined: 10/15/2021 Last visit: 4/29/2024 Posts: 3 Rating: (1) |
Hi bergmanu, Thank you again, I found some time to give it a try and it worked perfectly : Just in case someone needs it (to sum up) : How to install the Example Image on the IOT2050 Advanced's eMMC : 1) Change the boot order to have the mmc1 last
5) Copy the Example Image file onto another USB stick from the engineering station and then plug it into the IOT2050 6) Install the Example Image on the eMMC from the USB stick
7) Shutdown, unplug the USB stick / MicroSD and restart 8) Configure the IOT2050 with
9) Enjoy ! In the end, it was easier than I thought... Oh, and by the way, it was my potentiometer that was faulty... (and I had the wrong Node-RED nodes) Now everything is much clearer and works so far flawlessly :) AttachmentIOT2050 Advanced - Install on eMMC.zip (365 Downloads) |
Last edited by: QD13 at: 11/28/2021 17:21:05 |
|
This contribution was helpful to2 thankful Users |
Follow us on