12/2/2021 2:01 PM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
Please also see the attached screenshots. We have a machine with some nice pop-up displays showing what is blocking the machine from getting start permission. I can find the logic in the PLC and I can find the pop-up display in my Graphics editor in WinCC. But when I open the place where I thought the status tag would be linked to the bit from the DB (via a tag in the Tag manager) it is only telling me that "STATUS" is a missing tag - and this same tag is missing from all the tags in the pop-up display. I can see the numbering (from iLockStatus_0 to iLockStatus_15) in the "Object Name" for all the 16 bits used on the pop-up. I can see in the PLC and in the Tag manager that status is coming from DB101.DBD4 (so that is 32 bits) but how is this status transmitted to the pop-up display? AttachmentEB5 Interlock A.zip (156 Downloads) |
Follow us on