12/7/2021 11:00 AM | |
Joined: 3/11/2019 Last visit: 8/9/2024 Posts: 1550 Rating:
|
Hi Nikhil017, which revision of the gsd was downloaded? GSD revision 5 will not work with com profibus for example. PROFIBUS GSD files: ET 200S"The engineering tool used does not support GSD files with Revision 5, such as COM PROFIBUS" maybe this helps sancruz |
Feedback appreciated, please rate |
|
12/7/2021 2:39 PM | |
Joined: 3/11/2019 Last visit: 8/9/2024 Posts: 1550 Rating:
|
Hi, the GSD files has to be copied to COM PROFIBUS’s (...\gsd or ...\fmsgsd) directory. Afterwards please use menu bar -> file -> read gsd files. Afterwards the GSD should work. You can also read this in the manual: COM PROFIBUSBut as i can see, that you use GSD-files with DPV1 function. I'm not sure 100percent, but i assume that com profibus does not support this. You can also try an older GSD file from the same source, there are several versions available. PROFIBUS GSD files : ET 200Mregards sancruz |
Feedback appreciated, please rate |
|
Follow us on