12/18/2021 5:26 PM | |
Joined: 3/11/2021 Last visit: 3/15/2024 Posts: 5 Rating: (0) |
Good afternoon. An error occurred during the Starter installation. Help me.
Attachmenterror.zip (732 Downloads) |
12/20/2021 5:58 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
attach the logfile |
12/20/2021 7:17 AM | |
Joined: 3/11/2021 Last visit: 3/15/2024 Posts: 5 Rating: (0) |
The file that is attached to error.zip insufficient? |
12/20/2021 7:18 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
is the wrong one. please attach the two named in the errormessages |
12/20/2021 6:53 PM | |
Joined: 3/11/2021 Last visit: 3/15/2024 Posts: 5 Rating: (0) |
Look in this folder. All logs are there. If there is not, then write to me. AttachmentSetup.zip (693 Downloads) |
12/21/2021 4:16 PM | |
Joined: 3/11/2021 Last visit: 3/15/2024 Posts: 5 Rating: (0) |
Good evening. Help. |
12/25/2021 7:10 AM | |
Joined: 3/11/2021 Last visit: 3/15/2024 Posts: 5 Rating: (0) |
I attach the error log AttachmentInstallStarterLog.txt (554 Downloads) |
Follow us on