4/26/2021 11:02 PM | |
Joined: 2/22/2008 Last visit: 6/12/2024 Posts: 2698 Rating: (207) |
It is also possible to display RPM up to 300,000 with a little trick, but you need at least a Logo8 FS4 or a new Logo8.3, see attachment for example. In simulation just change I3 to frequency mode and type in 5000. The first multiplication by 6 is done with the arithmetic, 5000 x 6 = 30,000 is okay for this block. Multiplications by 10, 100 or 1000 you can make with the I/F and F/I converter. The eAQ output can be used in messages for higher values than 32767, but you cannot calculate with such values. Regards, Scorp AttachmentRPM300000.zip (641 Downloads) |
Follow us on