5/20/2021 2:27 PM | |
Joined: 4/28/2015 Last visit: 5/15/2024 Posts: 3345 Rating: (377)
|
Hi, yes, there is 20 Dx pins, which can be configured as DI or DQ. For a detailed overview and the possible function of each pin, see here. These pins work with 3.3 or 5V only; our Siemens I/O shield operates with 24V. If you are not requiring 24V you can use any other Arduino shield or use the pins directly (which is not very "industrial-like", because there are no screw termials). Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
1/18/2022 6:38 AM | |
Joined: 11/15/2018 Last visit: 5/23/2024 Posts: 20 Rating: (2) |
Hi, the link is not working anymore :-( other question: can the 10xDI shield 6ES7647-0KA02-0AA2 be mangaged in Node-red like the other one (5xDI, 2xAI, 2xDO) ? i mean, are all 10 DIs configurable with a DI-Node? thanks
|
Last edited by: Ursg at: 01/18/2022 06:38:51 |
|
Follow us on